Gadget Renesas

Linking Ideas and Electronics

GR Atelier

Title:PRESENTStick

Displayed Name:@takjn

PRESENTStick

Concept / Overview
Have you ever gone overtime, or finished too early, when giving a presentation or lecture?
This device uses the remaining slide number and time to calculate and inform you of how much time may be spent discussing each slide.
It can advance your slides (via Bluetooth) automatically, and allows you to pause, continue, or return to a previous slide manually.
####

The Idea & Happy Users

What characterizes an excellent presentation?

 

There is no definitive answer, of course, but there is one minimum requirement:
That is… to communicate your content within the allotted time.
No matter how excellent the presentation, if you cannot finish within the allotted time, the vital content will not be communicated.

 

PRESENStick is a presentation support device which prevents a “time-over” situation.
Input the number of slides and allotted time and the device will automatically calculate how much time you may use for each slide.
When the allotted time approaches, the emitted sound and vibration will urge the speaker to advance to the next slide.
The speaker may also manually pause, advance, or return to a previous slide.
Using the remaining slide count and time as a base, the device will recalculate the allotted time for each remaining slide.

 

That is precisely the world which PRESENStick seeks to promote.

 

PRESENStick creates the best situation for both speaker and audience.
The device is great for those who dislike public speaking and for those silver-tongued speakers who go off on tangents.
It helps ensure that the required content is communicated within the allotted time.
It facilitates a presentation satisfactory to both speaker and audience.

####

Demo Video

####

Source Code

The parts list, circuitry, and source code are open to the public.
https://github.com/takjn/presenstick

 

The breadboard prototyping protocol is also open to the public
https://github.com/takjn/presenstick/wiki/Prototyping

@takjn

GR Design Contest 2016 Finalist

share