Title:Lychee\'s awesome solution for Security and Health
Displayed Name:QTech
Concept / Overview |
---|
Home security is becoming necessary nowadays as the possibilities of intrusion are increasing day by day. Lot of Security companies are available towards protecting house from getting vandalized or so. But still there is no much guarantee. In addition there was a need to automate home so that user can take advantage of the technological advancement in such a way that a person getting off the office does not get melted with the hot climate.Then, when it comes to food,major question for farmers, ranchers, and food scientists around the globe is “How are we going to feed more than 9 billion people that will live on Earth by 2050?” In aquaponics there are some parameters like pH, temperature, EC(Electrical Conductivity), salinity and hardness are to be measured for achieving it. These parameters are measured using corresponding meters and sensors, then this output is fed to GR-Lychee.Similarly in home automation and security, the output of sensor and camera is given to GR-Lychee board. By using the feature of IoT in GR-Lychee, status is updated to user\\\'s mobile via android application wherever he/she may survive in the world. Not only monitoring the status user can also take action from anywhere in the world. With the help of one GR-Lychee user will become tension free about home and food. |

Overview
Razzle dazzle big puzzle, where will the global guzzle lead
us to! Technology is growing at an imaginable rate! With the advancement in technology, the number of electronic devices in our day-to-day Life has increased to make life simpler. But the dark side is that the rising population of India poses serious threats with regard to the availability of living space, utilization of natural resources and raw materials.
There is necessity to construct a trustable Remote System that will easily control all electronic devices in home from a distance. It will reduce both
• Complexity of handling the number of devices simultaneously,
• also power consumption.
Home security is also becoming necessary nowadays as the possibilities of intrusion are increasing day by day. Then, when it comes to food, major question for farmers, ranchers, and food scientists around the globe is “How are we going to feed more than 9 billion people that will live on Earth by 2050?” Increasingly, the quality of food is as important as quantity, and better food must become a priority.

Movie

Detail & Sources
GR LYCHEE Design Contest 2018 in India, Finalist